Hi Team,
Our customer bought the EVM module last month and after being used several times, the EVM module won't power up. The 5V LED would not turn on and the device could not be recognized by the customer's computer.
The customer tried powering up the EVM through the USB Connector (J1) and via the 5V power jack (J5) following section 2.7 of the datasheet to no avail. The customer also followed the recommended duty cycle of the sensor as stated on the datasheet and didn't do anything other than use the Webpage-based cloud analysis tool.
Could you help identify the issue with the module or if it is broken and eligible for a replacement?
Thank you.
Regards,
Marvin