Hello Scott,
There is application with 5 psi and 0-5V output, and 0 psi accuracy is critical, if I calibrate at 0-2.5-5.0 psi, there was always 0.1 psi error at 0 psi (it turns to very accurate after 0.15 psi). It works very accurately with 1-5V / 0.5-4.5V and 4-20mA output at 0 psi.
Can I calibrate 1.0-3.5-6.0 psi with ratiometric during DAC calibration, mark output 0-5 psi in EEPROM setting? or you have some other trickys.
Thank you in advance.
Ed