This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR6843AOP: Unable to building Labs in CCS, getting error during gmake

Part Number: AWR6843AOP
Other Parts Discussed in Thread: SYSBIOS

Hello TI Team,

I am trying to compile 68xx_people_counting project from industrial tool box version mmwave_industrial_toolbox_4_1_0. I am trying to compile it using SDK version mmwave_sdk_03_05_00_04. I am able to compile DSS project successfully, but while compiling mss project, I am getting gmake error. At first the postbuild process does not gets complete. It remain stuck at 43%. If I cancel the process then I get below error. I can be seen the compilation and xer4f file creation is successful. The process gets stuck at bin creation.

Request you to please offer solution to the issue.

I am using CCS Version 11.1.0


**** Build of configuration Release for project 68xx_pplcount_mss ****

"C:\\ti\\ccs1110\\ccs\\utils\\bin\\gmake" -k -j 12 all -O

rm -f C:/Users/rdicholkar/workspace_08March/68xx_pplcount_mss/xwr68xx_mmw_demo.bin
makefile:195: recipe for target 'pre-build' failed
process_begin: CreateProcess(NULL, rm -f C:/Users/rdicholkar/workspace_08March/68xx_pplcount_mss/xwr68xx_mmw_demo.bin, ...) failed.

gmake[1]: [pre-build] Error 2 (ignored)

Building file: "../mss_mmw.cfg"
Invoking: XDCtools
"C:/ti/xdctools_3_50_08_24_core/xs" --xdcpath="C:/ti/bios_6_73_01_01/packages;" xdc.tools.configuro -o configPkg -t ti.targets.arm.elf.R4Ft -p ti.platforms.cortexR:IWR68XX:false:200 -r release -c "C:/ti/ti-cgt-arm_16.9.6.LTS" --compileOptions "--enum_type=int " "../mss_mmw.cfg"
making package.mak (because of package.bld) ...
generating interfaces for package configPkg (because package/package.xdc.inc is older than package.xdc) ...
configuring mss_mmw.xer4ft from package/cfg/mss_mmw_per4ft.cfg ...
generating custom ti.sysbios library makefile ...
Starting build of library sources ...
making C:/Users/rdicholkar/workspace_08March/68xx_pplcount_mss/src/sysbios/sysbios.aer4ft ...
gmake[1]: Entering directory `C:/Users/rdicholkar/workspace_08March/68xx_pplcount_mss/src/sysbios'
gmake[1]: Nothing to be done for `all'.
gmake[1]: Leaving directory `C:/Users/rdicholkar/workspace_08March/68xx_pplcount_mss/src/sysbios'
Build of libraries done.
cler4ft package/cfg/mss_mmw_per4ft.c ...
Finished building: "../mss_mmw.cfg"

Building file: "../gtrackAlloc.c"
Invoking: Arm Compiler
"C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me -O3 --include_path="C:/Users/rdicholkar/workspace_08March/68xx_pplcount_mss" --include_path="C:/Users/rdicholkar/workspace_08March/68xx_pplcount_mss/common" --include_path="C:/ti/mmwave_industrial_toolbox_4_0_0/labs/people_counting/68xx_people_counting/src/mss/gtrack" --include_path="C:/ti/mmwave_industrial_toolbox_4_0_0/labs/people_counting/68xx_people_counting/src/common" --include_path="C:/ti/mmwave_sdk_03_05_00_04" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages" --include_path="C:/ti/ti-cgt-arm_16.9.6.LTS/include" --define=SOC_XWR68XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=MMWAVE_L3RAM_NUM_BANK=6 --define=MMWAVE_SHMEM_TCMA_NUM_BANK=0 --define=MMWAVE_SHMEM_TCMB_NUM_BANK=0 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN --define=APP_RESOURCE_FILE='<'mmw_res.h'>' -g --c99 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=int --abi=eabi --obj_extension=.oer4f --preproc_with_compile --preproc_dependency="gtrackAlloc.d_raw" --cmd_file="configPkg/compiler.opt" "../gtrackAlloc.c"
Finished building: "../gtrackAlloc.c"

Building file: "../gtrackLog.c"
Invoking: Arm Compiler
"C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me -O3 --include_path="C:/Users/rdicholkar/workspace_08March/68xx_pplcount_mss" --include_path="C:/Users/rdicholkar/workspace_08March/68xx_pplcount_mss/common" --include_path="C:/ti/mmwave_industrial_toolbox_4_0_0/labs/people_counting/68xx_people_counting/src/mss/gtrack" --include_path="C:/ti/mmwave_industrial_toolbox_4_0_0/labs/people_counting/68xx_people_counting/src/common" --include_path="C:/ti/mmwave_sdk_03_05_00_04" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages" --include_path="C:/ti/ti-cgt-arm_16.9.6.LTS/include" --define=SOC_XWR68XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=MMWAVE_L3RAM_NUM_BANK=6 --define=MMWAVE_SHMEM_TCMA_NUM_BANK=0 --define=MMWAVE_SHMEM_TCMB_NUM_BANK=0 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN --define=APP_RESOURCE_FILE='<'mmw_res.h'>' -g --c99 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=int --abi=eabi --obj_extension=.oer4f --preproc_with_compile --preproc_dependency="gtrackLog.d_raw" --cmd_file="configPkg/compiler.opt" "../gtrackLog.c"
Finished building: "../gtrackLog.c"

Building file: "../modules/utilities/cycle_measure.c"
Invoking: Arm Compiler
"C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me -O3 --include_path="C:/Users/rdicholkar/workspace_08March/68xx_pplcount_mss" --include_path="C:/Users/rdicholkar/workspace_08March/68xx_pplcount_mss/common" --include_path="C:/ti/mmwave_industrial_toolbox_4_0_0/labs/people_counting/68xx_people_counting/src/mss/gtrack" --include_path="C:/ti/mmwave_industrial_toolbox_4_0_0/labs/people_counting/68xx_people_counting/src/common" --include_path="C:/ti/mmwave_sdk_03_05_00_04" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages" --include_path="C:/ti/ti-cgt-arm_16.9.6.LTS/include" --define=SOC_XWR68XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=MMWAVE_L3RAM_NUM_BANK=6 --define=MMWAVE_SHMEM_TCMA_NUM_BANK=0 --define=MMWAVE_SHMEM_TCMB_NUM_BANK=0 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN --define=APP_RESOURCE_FILE='<'mmw_res.h'>' -g --c99 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=int --abi=eabi --obj_extension=.oer4f --preproc_with_compile --preproc_dependency="modules/utilities/cycle_measure.d_raw" --obj_directory="modules/utilities" --cmd_file="configPkg/compiler.opt" "../modules/utilities/cycle_measure.c"
Finished building: "../modules/utilities/cycle_measure.c"

Building file: "../modules/utilities/radarOsal_malloc.c"
Invoking: Arm Compiler
"C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me -O3 --include_path="C:/Users/rdicholkar/workspace_08March/68xx_pplcount_mss" --include_path="C:/Users/rdicholkar/workspace_08March/68xx_pplcount_mss/common" --include_path="C:/ti/mmwave_industrial_toolbox_4_0_0/labs/people_counting/68xx_people_counting/src/mss/gtrack" --include_path="C:/ti/mmwave_industrial_toolbox_4_0_0/labs/people_counting/68xx_people_counting/src/common" --include_path="C:/ti/mmwave_sdk_03_05_00_04" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages" --include_path="C:/ti/ti-cgt-arm_16.9.6.LTS/include" --define=SOC_XWR68XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=MMWAVE_L3RAM_NUM_BANK=6 --define=MMWAVE_SHMEM_TCMA_NUM_BANK=0 --define=MMWAVE_SHMEM_TCMB_NUM_BANK=0 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN --define=APP_RESOURCE_FILE='<'mmw_res.h'>' -g --c99 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=int --abi=eabi --obj_extension=.oer4f --preproc_with_compile --preproc_dependency="modules/utilities/radarOsal_malloc.d_raw" --obj_directory="modules/utilities" --cmd_file="configPkg/compiler.opt" "../modules/utilities/radarOsal_malloc.c"
Finished building: "../modules/utilities/radarOsal_malloc.c"

Building file: "../task_mbox.c"
Invoking: Arm Compiler
"C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me -O3 --include_path="C:/Users/rdicholkar/workspace_08March/68xx_pplcount_mss" --include_path="C:/Users/rdicholkar/workspace_08March/68xx_pplcount_mss/common" --include_path="C:/ti/mmwave_industrial_toolbox_4_0_0/labs/people_counting/68xx_people_counting/src/mss/gtrack" --include_path="C:/ti/mmwave_industrial_toolbox_4_0_0/labs/people_counting/68xx_people_counting/src/common" --include_path="C:/ti/mmwave_sdk_03_05_00_04" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages" --include_path="C:/ti/ti-cgt-arm_16.9.6.LTS/include" --define=SOC_XWR68XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=MMWAVE_L3RAM_NUM_BANK=6 --define=MMWAVE_SHMEM_TCMA_NUM_BANK=0 --define=MMWAVE_SHMEM_TCMB_NUM_BANK=0 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN --define=APP_RESOURCE_FILE='<'mmw_res.h'>' -g --c99 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=int --abi=eabi --obj_extension=.oer4f --preproc_with_compile --preproc_dependency="task_mbox.d_raw" --cmd_file="configPkg/compiler.opt" "../task_mbox.c"
Finished building: "../task_mbox.c"

Building file: "../cli.c"
Invoking: Arm Compiler
"C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me -O3 --include_path="C:/Users/rdicholkar/workspace_08March/68xx_pplcount_mss" --include_path="C:/Users/rdicholkar/workspace_08March/68xx_pplcount_mss/common" --include_path="C:/ti/mmwave_industrial_toolbox_4_0_0/labs/people_counting/68xx_people_counting/src/mss/gtrack" --include_path="C:/ti/mmwave_industrial_toolbox_4_0_0/labs/people_counting/68xx_people_counting/src/common" --include_path="C:/ti/mmwave_sdk_03_05_00_04" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages" --include_path="C:/ti/ti-cgt-arm_16.9.6.LTS/include" --define=SOC_XWR68XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=MMWAVE_L3RAM_NUM_BANK=6 --define=MMWAVE_SHMEM_TCMA_NUM_BANK=0 --define=MMWAVE_SHMEM_TCMB_NUM_BANK=0 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN --define=APP_RESOURCE_FILE='<'mmw_res.h'>' -g --c99 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=int --abi=eabi --obj_extension=.oer4f --preproc_with_compile --preproc_dependency="cli.d_raw" --cmd_file="configPkg/compiler.opt" "../cli.c"
Finished building: "../cli.c"

Building file: "../mss_main.c"
Invoking: Arm Compiler
"C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me -O3 --include_path="C:/Users/rdicholkar/workspace_08March/68xx_pplcount_mss" --include_path="C:/Users/rdicholkar/workspace_08March/68xx_pplcount_mss/common" --include_path="C:/ti/mmwave_industrial_toolbox_4_0_0/labs/people_counting/68xx_people_counting/src/mss/gtrack" --include_path="C:/ti/mmwave_industrial_toolbox_4_0_0/labs/people_counting/68xx_people_counting/src/common" --include_path="C:/ti/mmwave_sdk_03_05_00_04" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages" --include_path="C:/ti/ti-cgt-arm_16.9.6.LTS/include" --define=SOC_XWR68XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=MMWAVE_L3RAM_NUM_BANK=6 --define=MMWAVE_SHMEM_TCMA_NUM_BANK=0 --define=MMWAVE_SHMEM_TCMB_NUM_BANK=0 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN --define=APP_RESOURCE_FILE='<'mmw_res.h'>' -g --c99 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=int --abi=eabi --obj_extension=.oer4f --preproc_with_compile --preproc_dependency="mss_main.d_raw" --cmd_file="configPkg/compiler.opt" "../mss_main.c"
Finished building: "../mss_main.c"

Building file: "../task_app.c"
Invoking: Arm Compiler
"C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me -O3 --include_path="C:/Users/rdicholkar/workspace_08March/68xx_pplcount_mss" --include_path="C:/Users/rdicholkar/workspace_08March/68xx_pplcount_mss/common" --include_path="C:/ti/mmwave_industrial_toolbox_4_0_0/labs/people_counting/68xx_people_counting/src/mss/gtrack" --include_path="C:/ti/mmwave_industrial_toolbox_4_0_0/labs/people_counting/68xx_people_counting/src/common" --include_path="C:/ti/mmwave_sdk_03_05_00_04" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages" --include_path="C:/ti/ti-cgt-arm_16.9.6.LTS/include" --define=SOC_XWR68XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=MMWAVE_L3RAM_NUM_BANK=6 --define=MMWAVE_SHMEM_TCMA_NUM_BANK=0 --define=MMWAVE_SHMEM_TCMB_NUM_BANK=0 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN --define=APP_RESOURCE_FILE='<'mmw_res.h'>' -g --c99 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=int --abi=eabi --obj_extension=.oer4f --preproc_with_compile --preproc_dependency="task_app.d_raw" --cmd_file="configPkg/compiler.opt" "../task_app.c"
Finished building: "../task_app.c"

Building target: "68xx_pplcount_mss.xer4f"
Invoking: Arm Linker
"C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me -O3 --define=SOC_XWR68XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=MMWAVE_L3RAM_NUM_BANK=6 --define=MMWAVE_SHMEM_TCMA_NUM_BANK=0 --define=MMWAVE_SHMEM_TCMB_NUM_BANK=0 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN --define=APP_RESOURCE_FILE='<'mmw_res.h'>' -g --c99 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=int --abi=eabi --obj_extension=.oer4f -z -m"68xx_pplcount_mss.map" --heap_size=0x800 --stack_size=0x800 -i"C:/ti/ti-cgt-arm_16.9.6.LTS/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/control/mmwave/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/control/mmwavelink/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/drivers/crc/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/drivers/dma/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/drivers/esm/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/drivers/gpio/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/drivers/mailbox/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/drivers/osal/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/drivers/pinmux/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/drivers/soc/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/drivers/uart/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/utils/cli/lib" -i"C:/ti/mmwave_industrial_toolbox_4_0_0/labs/people_counting/68xx_people_counting/src/mss/gtrack/lib" -i"C:/ti/ti-cgt-arm_16.9.6.LTS/include" --reread_libs --disable_auto_rts --define=MMWAVE_L3RAM_NUM_BANK=6 --define=MMWAVE_SHMEM_TCMA_NUM_BANK=0 --define=MMWAVE_SHMEM_TCMB_NUM_BANK=0 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --diag_error=10015 --diag_warning=225 --diag_wrap=off --display_error_number --warn_sections --xml_link_info="xwr68xx_mmw_mss_linkInfo.xml" --rom_model --unused_section_elimination=on -o "68xx_pplcount_mss.xer4f" "./cli.oer4f" "./gtrackAlloc.oer4f" "./gtrackLog.oer4f" "./mss_main.oer4f" "./task_app.oer4f" "./task_mbox.oer4f" "./modules/utilities/cycle_measure.oer4f" "./modules/utilities/radarOsal_malloc.oer4f" "../mss_mmw_linker.cmd" "../r4f_linker.cmd" -l"configPkg/linker.cmd" -llibosal_xwr68xx.aer4f -llibesm_xwr68xx.aer4f -llibgpio_xwr68xx.aer4f -llibsoc_xwr68xx.aer4f -llibpinmux_xwr68xx.aer4f -llibcrc_xwr68xx.aer4f -llibdma_xwr68xx.aer4f -llibuart_xwr68xx.aer4f -llibmailbox_xwr68xx.aer4f -llibmmwavelink_xwr68xx.aer4f -llibmmwave_xwr68xx.aer4f -llibcli_xwr68xx.aer4f -llibgtrack2D.aer4f -lrtsv7R4_T_le_v3D16_eabi.lib -llibc.a
<Linking>
Finished building target: "68xx_pplcount_mss.xer4f"

C:/ti/mmwave_sdk_03_05_00_04/packages/scripts/ImageCreator/out2rprc/out2rprc.exe 68xx_pplcount_mss.xer4f 68xx_pplcount_mss.bin
Parsing the input object file, 68xx_pplcount_mss.xer4f.
Appending zeros 0
Appending zeros 256
Appending zeros 96968
File conversion complete!
C:/ti/mmwave_sdk_03_05_00_04/packages/scripts/ImageCreator/multicore_image_generator/MulticoreImageGen.exe LE 37 0x02000006 pplcount_lab_xwr68xx.bin 0x35510000 68xx_pplcount_mss.bin 0xb5510000 C:/ti/mmwave_sdk_03_05_00_04/firmware/radarss/iwr6xxx_radarss_rprc.bin 0xd5510000 C:/Users/rdicholkar/workspace_08March/68xx_pplcount_dss/Debug/68xx_pplcount_dss.bin

**** Build of configuration Release for project 68xx_pplcount_mss ****

!CommandLauncher.error.commandCanceled!
Error: Program "C:/ti/ccs1110/ccs/utils/bin/gmake" is not found in PATH

PATH=[C:/ti/ccs1110/ccs/eclipse/jre/bin/client;C:/ti/ccs1110/ccs/eclipse/jre/bin;C:\Windows\system32;C:\Windows;C:\Windows\System32\Wbem;C:\Windows\System32\WindowsPowerShell\v1.0\;C:\Windows\System32\OpenSSH\;C:\Program Files (x86)\NVIDIA Corporation\PhysX\Common;C:\Program Files (x86)\Webex\Plugins;C:\Program Files (x86)\PuTTY\;C:\WINDOWS\system32;C:\WINDOWS;C:\WINDOWS\System32\Wbem;C:\WINDOWS\System32\WindowsPowerShell\v1.0\;C:\WINDOWS\System32\OpenSSH\;C:\Users\rdicholkar\AppData\Local\Programs\Python\Python39;C:\Users\rdicholkar\AppData\Local\Programs\Python\Python39\Scripts;C:\Users\rdicholkar\Downloads\make-3.81-bin\bin;C:\Users\rdicholkar\AppData\Local\Programs\Python\Python39\Scripts\;C:\Users\rdicholkar\AppData\Local\Programs\Python\Python39\;C:\Users\rdicholkar\AppData\Local\Microsoft\WindowsApps;;C:\ti\ccs1110\ccs\eclipse;]

**** Build Finished ****