Hello, I am trying to connect AWR2243Boost with my PC but when I connect the board with USB, nothing appears in device manager. The power LED (5v) and NRST LED are on. I have also checked the PGOOD pin, and it also gave me 3.3 v. Is it the problem with firmware?
N.B. I have been using this board earlier and it was working fine but this time it stopped appearing in the device manager and the RS232 status in mmWave studio shows it is disconnected.