Other Parts Discussed in Thread: AWR1243
Hi,
Customer is encountering using the device, please see details below.
"I'm wondering if you'd be able to help me with a problem I have porting mmWaveLink for the AWR1243BOOST ES 2.0. I've been using the mmwavelink_example.exe program in mmWave DFP 1.00.00.01 (the last DFP/SDK version compatible with ES 2.0 AWR1243), but I decided to implement the callback functions in the porting guide so that I could port it to whatever system it might need to be used with in the future. After doing so, however, the AWR1243 doesn't respond consistently. The host interrupt doesn't go high even after setting nReset low, waiting for various amounts of time (1-2000 ms), and setting it high again, except in a few cases when I either waited for a few minutes or unplugged and restarted the device. I also tried ignoring the host interrupt and triggering the interrupt callback as if it had gone high, but then mmwavelink failed to detect any header or sync packets on SPI.
The closed source library provided in the DFP works fine, but I'm not sure what to do since I'm not aware of any other steps to implement the callback functions. Is there anything I might not be doing right or might not be aware of?"
Regards,
Maynard