Other Parts Discussed in Thread: AWR1843
I am aware of the fact that around 150kmh is the max speed measurable with AWR1843Boost. We also note that some companies like Smartmicro and Oculii claim 300kmh max speed measuring capability with single AWR1843. I played with some parameters in the mmWave Sensing Estimator, single Tx, four Rx (no need for a total beam angle more than 30 degrees, no need for beam forming), low range resolution, low velocity resolution and found out that max. speed up to 300kmh is possible. Checked all parameters and no errors found. Is there something that I ignored? Thank you.