This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843: SDK contents

Part Number: AWR1843

Hello, I have something to ask about the SDK User Guide.

Below is the text of the SDK User Guide
-------------------------------------------------- -------------------------------------------------- ----------------------------------------
4. 5. 3. Building demo
To clean build a demo, first make sure that the environment is setup as detailed in earlier section. Then run the following commands. On successful
execution of the commands, the output is <demo> .xe * which can be used to load the image via CCS and <demo> .bin which can be used as the binary
in the steps mentioned in section "How to flash an image onto mmWave EVM".
-------------------------------------------------- -------------------------------------------------- ----------------------------------------

I don't know the specific effective command here.
I would appreciate it if you could tell me.