Thank you for your help.
Currently, we are making a prototype of an eddy current sensor using LDC0851.
Please tell us about the following.
question:
At LDC0851_Stacked_design Manual Section 4.3
The explanation in this section states that a ferrite material cannot be used for the shield of the sensing coil.
Is this because it is a ferromagnet?
For shield Should I use a non-magnetic material?
Or with a magnetic material There is stainless steel
Is it possible to use?
That's all, but your answer
Thank you for your cooperation.