This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi community member,
My customer would like to evaluate 2 cascade using TI EVM.
However, I can't find how to connect 2 cascade from any guide.
Please let me know any guide how to connect 2 cascade if TMDS273GPEVM can connect with AWR2243BOOST.
Best regards.
Cruijff
Hi,
can you please clearly mention which kits/EVM's you are referrring here?
We have a EVM of AM273 which has 60 pin connector to mate to AWR2243BOOST.
Regards
Hi,
You can connect 2 separate 2243BOOST EVM to TPR12 EVM but the important point is what all you would need to make them work. You cannot operate them in cascade as there is no FMCW sync(20GHz LO) between the 2 frontends. Even to operate the AWR2243 BOOST connected on second 60pin connector you will have to make changes in the example code for SPI and nRST.
Regards