This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOP: About the accuracy in the level_sensing lab

Part Number: IWR6843AOP


Hi expert,

We are working on a project in which the range bias has to be controlled with in ±2mm when detecting a large target in 2~40m.

And the level sensing lab seems to be a good start point. Would you guys help in the following questions:

1. How to calculate the resolution for the zoom-fft used in the level sensing project?
2. Is AoP capable of detecting a large object in 40m?

Thanks

Tony