Hello,
we are looking to TMP117 as possible replacement for thermistors.
Graphs at paragraph 6.9 of the datasheet already provide useful info about accuracy but I have a few additional questions, specifically for temperature range 10-40°C.
If I take one TMP117 sensor with its own error characteristic, how much of the error could be an offset and how much could be a slope error?
In other words, if a sensor has 0.08 (for example) accuracy, can it have error of +0.08 at 10°C and -0.08 at 40°C?
Would the slope be somehow constant or could the sensor show many ups-downs within the accuracy bandwidth? (always in range 10-40°C)
And if I take more TMP117, how much could the slope error be spread among them?
Any clarification related to these questions would be welcome.
Thank you, Lorenzo Merlo