This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOP: Questions about the Level Sensing lab

Part Number: IWR6843AOP


Hi expert:

We found that there was only one peak in the x-y scatter plot of the level sensing project, which is supposed to be 3 peaks as illustrated as the document in that project.

Our setup is:
1. AoP 6843
2. Corresponding firmware (68xx)
3. The default configuration file (0.3~3m)
4. ITB 4.10
5. Visualizer launched from the document

The question is where we can find the visualizer (with 3 peaks as seen as in the doc)?