This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: Execute DC-term calibration just once after radar installation

Part Number: AWR1642


We would like to execute DC-term calibration just once after radar installation.

The reason is that Radar might reflect by body of vehicle while Radar install on the surface of vehicle.

More, we will request customer clear environment (No metal objects) around 150cm then doing calibration (Issue CLI command "calibDcRangeSig -1 1 -5 25 128") after Radar installation.

Since the result of DC-term calibration cannot be recorded by current profile design, is there any good way to do?

Thanks a lot.

Best,

From RoyalTek Richard Lin.

http://www.royaltek.com/