This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP117:At high temperature, TMP117 temperature acquisition problem

Part Number: TMP117


Hello TI Engineers :

We apply TMP117MAIDRVR to constant temperature PCR machine, which is accurate at low temperature (such as 42°C), but when we keep constant temperature at 62°C, temperature acquisition is inaccurate. I hope you can assist our .

  • Dear Fred - 

    Thanks for the post! Here you will need to give us a bit more detail about your problem as this part is ±0.15C accurate in that temperature range. 

    I would suggest you share details that you can on the schematic, the layout and even the code snippet from you converting the output of the device to C, then we should be able to quickly get back to you will helpful suggestions towards resolution of your problem.