Hello,
i try to make use of the wakeup & sleep mode of the TMAG5273. My device configuration looks like this:

According to this configuration i would expect that the device wakes up every 100 ms and generates an interrupt after the conversion of XYZ is complete. But no interrupt is generated, even when i wait several seconds. When i use the device in continuous conversion mode it works fine including interrupt generation. What do i have to do to make the W&S mode work?
Thanks
A. Sengespeick