Hi expert,
The customer's questions are as follows:
Jiahui
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi expert,
The customer's questions are as follows:
Hello Jiahui,
What kind of device/board are you using?
Thanks,
Ehtesham Shareef
To answer your question,
It would be Unlikely and very hard to use a self-designed waveform. The reason for this that there are various other timing parameters (Frame generation signals, ADC start time, ADC valid time etc ) so closely coupled with the Synthesizer signal and they interconnect. Timing correlations are done with the help of Ramp generator state machine and BSS firmware. It would be very hard to time synchronize all those signals w.r.t to external LO (Ramp generator) synchronized.
Thanks
-Shareef
Hi expert,
Thank you for your quick reply.
There is no specific board. The customer wants to do his own research and use his own waveform.
I'll give your suggestion back to the customer and see what he reply.
Thanks!
Best Regards,
Jiahui
Hi expert:
Thsnks for your answer.
Your concerns in the answer are mostly about timing and synchronization.
What if the timing and synchronization are done through an external CLK. For example, we use a USRP to generate OFDM waveform which is fed into the TI mmWave radar product. At the same time, our USRP and the TI mmWave radar product use a single external CLK or oscillator.
I wonder if there are some interfaces reserved for the upper mentioned functionality.
Wish for your reply.
Much thanks.
Best Regards,
Jiahui
Let me reach out to the expert on this subject and get back to you.
-Shareef