This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944EVM: Stream ADC data through ethernet

Part Number: AWR2944EVM

Hi,

Is it possible to stream ADC data through the onboard ethernet to a PC. What would be the maximum frame rate? are they some sample code to do that?

For your information, I do not plan to use the DCA1000EVM

Thanks

Julien

  • Hi Julien,

    The out of box demo in SDK 4.2.0.2 (and 4.2.0.3 released recently) has an ethernet streaming variant that streams pointcloud data over ethernet. This can be modified to instead send ADC data.

    The framerate would be dependent on the kind of frame, I won't be able to give a number as we have not explored the maximum ethernet throughput in the OOB demo application.

    Regards,

    Aayush