Dear TI Team,
please can you provide thee absolute gain of the RX antennas in dBi. In Figure 7.2/7.3 the values are standardized to 0dB which helps here.
Thanks
Jens
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI Team,
please can you provide thee absolute gain of the RX antennas in dBi. In Figure 7.2/7.3 the values are standardized to 0dB which helps here.
Thanks
Jens
Hi,
The measurements provided in Figure 7.3 are measured using a Corner Reflector placed at 3-4m from sensor. The gain is measured from the captured raw data.
This is the reason why, for this type of measurement the absolute gain does not have meaning.
Thank you
Cesar
Hi Cesar,
a little more information: I would like to calculate a link budget in terms of SNR, where I need to know the absolute antenna gain. With this I will calculate the SNR at the IC input, through the LNA and after the FMCW algorithm. The reason for this is a performance comparison of the AoP and the non-AoP device for radar projects in general.
Thank you!
Johannes
Hi,
Yes, sorry for the delay
For AWR1843AOP the information available is provided in the datasheet.
Section 7.7 RF Specification.
We don't have any other information available
thank you
Cesar