This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843AOP: Beam steering, Raw data collection and velocity calculation

Part Number: AWR1843AOP
Other Parts Discussed in Thread: AWR1843BOOST, , , AWR1843

1) For beam steering how to decode the Raw Data coming from the Sensor, we are using the pre-built binary inside the MRR beam steering folder within the automotive toolbox for our experiments we don’t want to use the GUI (Matlab based which doesn’t have log function) so we are using serial monitor tool to collect the data, we need to know how to decode it
2) While searching we found the document where TLV format was mentioned, we want to know little bit more about the parameters defined in the format example (there is a parameter called peak value, we don’t know peak value of what ?)
3) We are doing beam steering from -60 deg to +60 deg with a step size of 120 Degree, we didn’t get any frame, object detected and object related information we used to get from the Out of Box demo
4) Beam steering is there a way to log which object is detected from which angle (in our case from -60 Deg or +60 Deg)
5) Beam Steering time of 60ms is defined in the document per angle, can we reduce it if we work on the chirp parameters ?
6) Which variable and how to get the relative velocity within the BeemSteering application?

  • Hi,

    Are you using a AWR1843AOP EVM or AWR1843BOOST EVM?

    The beamsteering demo is not supported on the AWR1843AOP EVM

    Thank you

    Cesar

  • Yes Cesar, i am using AWR1843AOPEVM, i used the prebuilt binary found within the automotive toolbox (attached folder snip below),

    are you saying beamsteering is not supported by this AOP IC ? or Beamsteering is not implemented in the provided prebuilt binary within the toolbox ?

    what needs to be done to make the beamsteering work on the AWR1843AOPEVM module ? 

    Regards

    Prince. A

  • Is it a mandate to use AWR1843BOOST EVM to get the beam steering (beamforming ) implemented ?

  • Yes, beam steering is not supported on AWR1843AOP SDK demo.

    Can you please provide more details about your application?

    The AWR1843AOP is targeted for near field sensing applications with a range up to 50m.

    For applications that require longer range we usually recommend AWR1843 with PCB antennae

    thank you

    Cesar