The newest mmwave sdk (3.5.0.4) is over a year old now. Some of the sdk libraries have been copied into more recent toolbox releases, and even updated. For instance, the SDK 3.5.0.4 version of aoaprocdsp does not support the AOP chip - only the separate aoa2dproc library supports AOP (and for hwa only, no dsp support). However, an updated version of aoaproc can be found in the Industrial Toolbox which has combined the two (aoaproc and aoa2dproc) into a single aoaproc library. And this Toolbox version of aoaproc does include both hwa and dsp support for the AOP chip. aoaproc is not the only sdk library which has been copied to the Toolbox and updated.
The Toolbox does not include doxygen updates for these libraries as far as I can find.
Is there an updated sdk release which includes the newer copiies of the libraries, along with updated doxygen files? Or, is there at least updated doxygen somewhere?