This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: Emulation package error

Part Number: IWR1642BOOST
Other Parts Discussed in Thread: IWR1642

Hi,

I bought the fully set up IWR1642Boost board, however, I am trying to run the traffic monitoring demo and I am unable to get it to collect data via the gui or the CCS

in CCS this is the error I am getting, CS_DAP_0: Error connecting to the target: (Error -261 @ 0x0) Invalid response was received from the XDS110. (Emulation package 9.6.0.00172

Is there a way to resolve this problem? I am not sure what to do, am I able to get a replacement board if this isn't fixable, I just bought it.

Thanks,

Jessica