This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: Not receiving UART signals in mmwave demo

Part Number: IWR1443BOOST
Other Parts Discussed in Thread: IWR1443

Howdy,

I am currently using the IWR1443boost flashed with the out of box demo for a project. I can run the demo succesfully over using the mmWave Demo Visualizer and can view and record the raw data in my computer terminal but when I disconnect the radar from my computer it stop outputting data. I believe this is because the computer is hosting the radar and when the host is removed it won't continue sending data. I would like to resolve this issue by setting up UART communication between the radar and the MSP432 which I am using for my project. I have searched through the mmwave demo visualizer source code and it looks like UART communication is already established but I cannot find UART outputs in any of the headers. Is it possible to set up UART communication from the IWR1443 and if so is there a project that I look over to learn how to do this. 

Thank you,

Daniel Jackson