This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843:IWR6843

Part Number: IWR6843
Other Parts Discussed in Thread: IWR1843, , IWR1642, IWR1443

Hello Sir,


First of all, because I am an overseas user, this text uses a translation site.
Therefore, there may be mistranslations.
I appreciate your understanding in advance.

Until now, we have been developing using IWR1843.

However, it may be developed with IWR6843, IWR1642 and IWR1443 in the future.

In the above, is the output data format of IWR6843 etc. common to that of IWR1843?

Also, please let us know if there are any differences other than the output data format.

Thanks for your support.
Regards,

  • Hi Ryota, 

    The output data format for the devices running on SDK 3.5 (i.e. IWR16xx, IWR18xx, IWR64xx, IWR68xx) have the same output data format.  This can be found in the mmWave SDK 3 Doxygen under the section titled "Output Information Sent to Host."

    file://<INSTALL_LOCATION>/mmwave_sdk_03_05_00_04/packages/ti/demo/xwr64xx/mmw/docs/doxygen/html/index.html

    The output data format for the IWR14xx, which runs on SDK 2.1 can be found in the SDK 2 Doxygen under the section titled "Output Information Sent to Host."

    file://<INSTALL_LOCATION>/mmwave_sdk_02_01_00_04/packages/ti/demo/xwr16xx/mmw/docs/doxygen/html/index.html

    Regards,

    Brennan