Other Parts Discussed in Thread: SYSBIOS, UNIFLASH, IWR1843, IWR6843
Hi,
sorry if I've asked this before - there's a lot to learn between tools, sysBios, applications etc !
Once I have a successful build in CCS (e.g OOB demo as a known starting point, before I try my own code), I can download & debug in CCS - but what if I want to configure & use the system via say mmWaveStudio, with code from CCS?
mmWaveStudio requires a file (e.g. ...MASTERSS.bin) to be downloaded, overwriting the CCS debug load.
>> How do I turn the CCS output - which I assume has separate MSS & DSS parts, into one file which contains both (presumable MASTERSS is both)?
Is this done with Image_Creator, or is that just for FLASH files ... or are FLASH files & those suitable for mmWavewSTudio the same? In the image_creator doc, it says something about the SDK may contain tools - is there a simple way to use it?
Or, if its not image_creator, how do I do this?
may thanks
Alan Milne