Hello,
I am using Traffic Monitoring from the industrial toolbox v4.10.1.
The documentation for people counting (which is meant to be referenced for TM tuning purposes too) says the following about the sensorPosition command:
Why is the azimuth tilt adjustment not supported? I've noticed that the tracking precision is greatly impacted by the azimuth sensor tilt.
If I want to monitor, say, an intersection from a corner, should I try to keep the sensor as straight as possible and limit the FOV via the boundaryBox command? Or should I just tilt the sensor without doing any configuration adjustments?