This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843: Maximum CANFD message ID number question.

Part Number: AWR1843


Hi team,

In AWR1843 TRM, chapter 23.1.2.11.6, It said that extend message ID filter Element, Up to 64 filter elements can be configured for 29-bit extended IDs

Question:

Is the 64 filter elements means we only support up to 64 specify ID in CANFD driver for both RX/TX?

Or it means it can support 64 sector of the CANFD ID? Then specify ID can larger than 64?

Thanks.

Regards,

Wesley