This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243BOOST: How to use the rlSetChannelConfig API ?

Part Number: AWR2243BOOST
Other Parts Discussed in Thread: AWR2243
Hi,
Does rlSetChannelConfig API work on awr2243?
How can I fix this error? 
Thanks
-----------------------------------------------------
platform:
am273x + awr2243 EVM
API:
retVal = rlSetChannelConfig (RL_DEVICE_MAP_INTERNAL_BSS, &ptrMMWaveMCB->openCfg.chCfg);
error messages:
==============================
Error: setChannelConfig retVal=-2
Set mmWave Link Channel Config Fail
==============================
  • Hello Kris, 

    Please give us some time to review your concern and we will get back to you within 24hrs. 

    Regards,

    Ishita

  • Hi,

    rlSetChannelConfig() is one of the fundamental mmWave Link APIs. It is supported in all the AWR2xxx mmWave link releases.

    What dfp version are you using?

    Based on error it seems that there is an issue sending the command.

    Are you able to send other commands?

    Thank you

    Cesar

  • Hi Cesar,

    Here are the steps.

    ========================

    1.Power up ...
    2.Use API:
    rlSetChannelConfig();
    rlSetAdcOutConfig();
    rlSetLowPowerModeConfig();
    rlRfInit();
    rlSetContModeConfig();
    ========================
    It works on SoC(xwr1642, xwr1843)  above.
    I'm not sure how to get the version from awr2243 exactly.
    I try to flash the firmawres to awr2243 by using mmWave studio.
    Is this method correct?
    Thanks.

  • Hi,

    Please follow the steps as numbered on the button of Studio GUI.

    Looks like you might missed to clock on RF power-up button and directly jumping on channelconfig Button which is returning -2 error.

    Optionally you can try running LUA script

    C:\ti\mmwave_studio_03_00_00_14\mmWaveStudio\Scripts\DataCaptureDemo_xWR.lua 

    where it loads the firmware first over RS232 in SOP2 (development mode).

    I'm not sure how to get the version from awr2243 exactly.

    When you clock on RF Power-up (as follow the ordered button numbers) then GUI will populate the version on the screen.

    I try to flash the firmawres to awr2243 by using mmWave studio.

    mmWave Studio works in SOP2 (development mode) where firmware (BSS and MSS) are loaded over RS232. In SOP2 mode, flashing is not possible.