This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944EVM: AWR2944EVM

Part Number: AWR2944EVM
Other Parts Discussed in Thread: AWR2944

Hi,

  We have been trying to flash the desired appimage into the device as per the instruction provided in the sdk user guided.

The procedure was  very confusing. We some how managed to do the procedure as per the instruction. We have edited the default.cfg  file  , and replaced the dfault path to our appimage path, and tried flashing the image. But it always showed a parsing error . The error is showing the line whwre the path is set. 

Can anyone help me resolve this issue?

Regards

Sreenath

  • Hi Sreenath,

                       One thing to check is if you have set the environment variables before the appimage was flashed. Ideally you would need to setenv.bat file using a cmd prompt in C:\ti\mmwave_mcuplus_sdk_04_02_00_02\mmwave_mcuplus_sdk_04_02_00_02\scripts\windows and navigate back in the same cmd prompt and then flash the image as per the procedure. Also, make sure the device type is set to awr2944 in setenv.bat file.

                       Let me know if you have any questions.

    Thanks and Regards,

    Akshay.