This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BOOST-LDC3114EVM: Integration with DRV2604L

Genius 17625 points
Part Number: BOOST-LDC3114EVM
Other Parts Discussed in Thread: DRV2604L, LDC3114

Hi Experts,

Seeking your assistance for this query:

I want to integrate DRV2604L into my project, as well as to be able to test its features with the www.ti.com/.../HAPTICS-CONSOLE. However, I need to buy an Evaluation module to do that and I dont want to buy yet another EVM module. I have recently bought a LDC3114 EVM which has MSP430 board on it (PAMB). Can I use this PAMB Board to connect it to DRV2604L and drive it via Haptics Console?

Thank you!

Regards,
Archie A.

  • Hello Archie, 

    The PAMB is flashed with firmware to communicate with the LDC3114EVM and it's GUI by default and is not setup to support the Haptics Console. You could still drive the DRV2604L using the PAMB but would have to modify the firmware and re-flash the PAMB for your specific implementation. 

    Best Regards, 

    Justin Beigel