This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOPEVM: MIMO scheme

Part Number: IWR6843AOPEVM

Hello,

I have used the mmWave_Demo_Visualize_3.5.0 generated several configurations for the sensor IWR6843AOPEVM. 

But I do not know how to recognize which kind of MIMO multiplex scheme is used for specific configuration: TDM or BPM

Below is a setting of 4Rx-3Tx

% ***************************************************************
% Created for SDK ver:03.05
% Created using Visualizer ver:3.5.0.0
% Frequency:60
% Platform:xWR68xx_AOP
% Scene Classifier:best_range_res
% Azimuth Resolution(deg):30 + 30
% Range Resolution(m):0.044
% Maximum unambiguous Range(m):9.02
% Maximum Radial Velocity(m/s):1.21
% Radial velocity resolution(m/s):0.16
% Frame Duration(msec):100
% RF calibration data:None
% Range Detection Threshold (dB):15
% Doppler Detection Threshold (dB):15
% Range Peak Grouping:enabled
% Doppler Peak Grouping:enabled
% Static clutter removal:disabled
% Angle of Arrival FoV: Full FoV
% Range FoV: Full FoV
% Doppler FoV: Full FoV
% ***************************************************************
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 7 0
adcCfg 2 1
adcbufCfg -1 0 1 1 1
profileCfg 0 60 287 7 57.14 0 0 70 1 256 5209 0 0 158
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 2
chirpCfg 2 2 0 0 0 0 0 4
frameCfg 0 2 16 0 100 1 0
lowPower 0 0
guiMonitor -1 1 1 0 0 0 1
cfarCfg -1 0 2 8 4 3 0 15 1
cfarCfg -1 1 0 4 2 3 1 15 1
multiObjBeamForming -1 1 0.5
clutterRemoval -1 0
calibDcRangeSig -1 0 -5 8 256
extendedMaxVelocity -1 0
lvdsStreamCfg -1 0 0 0
compRangeBiasAndRxChanPhase 0.0 1 0 -1 0 1 0 -1 0 1 0 -1 0 1 0 -1 0 1 0 -1 0 1 0 -1 0
measureRangeBiasAndRxChanPhase 0 1.5 0.2
CQRxSatMonitor 0 3 5 121 0
CQSigImgMonitor 0 127 4
analogMonitor 0 0
aoaFovCfg -1 -90 90 -90 90
cfarFovCfg -1 0 0 8.92
cfarFovCfg -1 1 -1.21 1.21
calibData 0 0 0
sensorStart

My questions:

1. With which attribute can I recognize the MIMO multiplex scheme?

2. I have also let the mmWave_Demo_Visualize generated a setting for 4Rx-1Tx, and the range resolution and speed resolutions and ambiguities stay unchanged. What is the cost by setting 3Tx? Which performance is then compromised by using 3Tx setting? Otherwise, we can also use the 3Tx-4Rx as default, since it provides the best angle performance.

3. There are many configuration attributes. Where can I find their descriptions about how I can interpret them and change them?