Hello,
Can you please tell me what is the meaning of this difference explained in the datasheet? "In order to meet the matching specification of the LMT70A, two units must be picked from adjacent positions from one tape and reel. If PCB rework is required, involving the LMT70A, then the pair of the LMT70A matched units must be replaced. Matching features (which include, without limitation, electrical matching characteristics of adjacent"
Does that mean the fact that the placement on the tape is different than LMT70? or is it just a difference of the temperature tolerance?
Thank you!