Other Parts Discussed in Thread: AMC1300, DRV425
Dear team,
My customer would like to consider to use TMCS1101A4B/U: 400 mV/A for AC current sensing application.
Their target resolution is 50mA. I think TMCS1101 would meet their target If ADC resolution is enough. But my concern is offset error of TMCS1101A4B/U
At datasheet, the max offset voltage of TMCS1101A4B/U is 28mV,
If the customer use TMCS1101A4B/U : 400 mV/A, the output voltage corresponding to 50mA is 20mV. Is it right?
The offset error is likely to cause output error. Please let me know your opinion on this concern.
Please let me know if TMCS1101 is not right device. If TMCS1101 is not right device for customer application, please recommend right solution.
Thank you.