Hi,
This is the same question that was not answered in my last thread.
I'm copying the question below.
From the DCA1000 user guide, it says: "LVDS data rates support a maximum of 600 Mbps. It supports both 4 lanes (xWR1243/1443) and 2 lanes (xWR1642)." Could you please confirm if the 600 Mbps is for four-lane together, or for each lane (so that total becomes 600x4=2.4 Gbps)?
Thanks,
Ham