This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1843BOOST: IWR1843BOOST

Part Number: IWR1843BOOST

Doesn't look like I've attached all I wanted to - try again.

/ti/mmwave_industrial_toolbox_4_9_0/labs/out_of_box_demo/18xx_mmwave_sdk/prebuilt_binaries/isk/xwr18xx_mmw_demo_isk.bin

magic word: 5254534D
metaimages present: 00000003
file length: 0004EA80h = 322176d
MSTR/MEND Protocol OK

MetaImage 1 details:
    filePresent = 0001
    coreId        = 35510000 >>> MSS
    fileOffset     = 0080
    CRC_lo       = EA7A2C43
    CRC_hi       = 69F4A22
    fileSize        = 1EB78
    reserved_1 = 0000
    reserved_2 = 0000

MetaImage 2 details:
    filePresent = 0001
    coreId        = B5510000 >>> BSS
    fileOffset     = 1EC00
    CRC_lo       = D05D7A98
    CRC_hi       = 5C1A98BA
    fileSize        = 8840
    reserved_1 = 0000
    reserved_2 = 0000

MetaImage 3 details:
    filePresent = 0001
    coreId        = D5510000 >>> DSS
    fileOffset     = 27440
    CRC_lo       = EF45D441
    CRC_hi       = 12ED896C
    fileSize        = 27630
    reserved_1 = 0000
    reserved_2 = 0000

MetaImage 4 details:
    filePresent = 0008
    coreId        = 444E454D >>> INVALID
    fileOffset     = 43525052
    CRC_lo       = 17610
    CRC_hi       = 0000
    fileSize        = 0004
    reserved_1 = 0001
    reserved_2 = 0000

Shared memory word: 0008




<34><00><BC><F7><FF><09><17><00> : <53><00><94><38><30><00><31><9C>
<00><34><A4><00><34><52><AD><F5> : <B4><3A><30><00><31><BC><00><34>
<C4><00><34><22><31><35><D4><3C> : <30><00><31><7C><32><7F><C9><38>
<1F><7C><8A><7D><F4><FE><FF><E6> : <EA><7E><F3><7F><7F><02><FF><E6>
<99><30><14><F0><49><74><67><75> : <1A><07><00><01><FF><F0><00><00>
<85><6E><01><00><25><7F><01><00> : <93><D3><01><00><00><00><00><00>
527: {Write to Sram}  metaImage number: 1 metaImage type: 4
chunk: 524 Remainder 
 bin file addr: 0001EBC0
<AA><00><3B><F3><26>
<00><00><00><00><3C><33><00><00> : <00><00><00><00><00><08><00><00>
<00><00><00><00><00><80><00><00> : <E8><E6><01><00><40><B3><00><08>
<88><EB><01><00><00><80><00><08> : <90><EB><01><00><50><D6><00><08>
<98><EB><01><00><00><00><00><08> : 
528: {Close to Sram}
<AA><00><07><04><22><00><00><00><04>
211: {Open to Sram} image ID: 2 metaImage type:5
<AA><00><13><D1><21><00><00><88><40><00><00><00><04><00><00><00><05><00><00><00><00>
530: {Write to Sram}  metaImage number: 2 metaImage type: 5
chunk: 0 bin file addr: 0001EC00
<AA><00><F3><FB><26>
<52><50><52><43><31><00><08><00> : <00><00><00><00><03><00><00><00>
<01><00><00><00><00><00><00><00> : <00><00><08><00><00><00><00><00>
<24><00><00><00><00><00><00><00> : <00><00><00><00><00><00><00><00>
<E7><10><CF><D0><ED><AD><10><D0> : <02><00><00><01><11><0A><05><00>
<00><00><00><00><31><00><08><00> : <01><02><06><0B><14><06><02><00>