This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDC2214: Drive current setting

Part Number: FDC2214


Hello,

I'm testing a new design based on the FDC2214 and I am tuning the drive current setting. 

We use a 39pF capacitor and 22uh inductor. (we want to measure ~0-100pF)

We only use 1 channel and use a 32MHz external clock. 

When I have no load atatched I can tune the amplitude pretty well and within 1.2V - 1.8V. (best setting is about 13 and 108uA). 

When I connect some cappacitance to the output the amplitude increases and even with setting 1 so 18uA the ampltitude is about 2.2V, which is higher than the datasheet recommends.  

I do use a driven shield which uses a BUF634AIDR as buffer and this signal is buffered and connected to the shield of the coaxial cable that carries the signal. 

The driven shield signal is a good representation of the input signal with minimal phase shift. 

What could we adjust to get the output voltage in the correct range?

Thanks in advance. 

  • Hello, 

    You can add a parallel resistor to your LC tank in order to change the amount of current required to drive your sensor within the recommended range. You may have to test with different resistors if you cannot quantify the current Rp of your LC tank with the load attached. In general, going above the 1.8V limit can lead to a reduced measurement accuracy over temperature while going below the 1.2V limit can increase the SNR. It is okay to go below the 1.2V limit during operation as long as you are still meeting the measurement resolution requirements of your design. 

    Best Regards, 

    Justin Beigel