This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: AWR2243 SFLASH not working for cascade example

Part Number: AWR2243

I created this post because the last post (e2e.ti.com/.../awr2243-unknown-error-response) I was trying to solve a different problem, but in an attempt to solve it I was running the FLASH example but it would not permanently flash the FW with the latest load, through the use of the AWR_DEV_FILE_DOWNLOAD_SB and setting the device management mode to SOP5.  I was wondering if there is an erase command that is needed or if I am missing a step in order to permanently place the patch version into flash so if will boot up without having to send this message.

Thank you