Hello,
I am now working on a modified Out of the Box Demo for the AWR1642BOOST, but I was wondering if it is possible to start the sensor right away when it is powered? When I modified the code, it is still need to be configured from the MmWave DemoVisualizer, so can you give me a starting point where the modification should be done in order sensor to start when it is powered with a hard coded configurations?
Any feedback would be appreciated.
Thanks in advance,
Beril.