Other Parts Discussed in Thread: TIDA-060024, ,
Hi Team,
Our customer uses a formula of “Jaju747” and “slaa732a” to calculate "CTUNE ".
However, typical values for tuning capacitance ranges is different.
- Jaju747 / 2.2.5.1 Tuning Capacitor / Typical values for the tuning capacitance range from 50 pF to 5000 pF.
-slaa732a / 4.4.2 Tuning Capacitor / Typical values for tuning capacitance ranges from 100 pF to 2000 pF.
And, "CTURN" and "RDAMP" are different depending on the document.
Even if “TDK EPCOS B78416A2232A003" and " MURATA MA58MF14-7N" are the same combination.
- TIDA-060024 / CTUNE=0.68nF,RDAMP=10kΩ
- BOOSTXL-PGA460 EVM / CTUNE=1500pF,RDAMP=2.7kΩ
And, these values are different from the their calculation result of “CTURN”.
They have two questions.
--------
[Q1]
Is there any material that explains the introduction process and theory of the formula "CTURN"?
And, which "typical values for tuning capacitance ranges" is correct(better), "Jaju747" or "slaa732a"?
[Q2]
Could you please let us know the measurement method (circuit) of the parasitic inductance of the transformer of “CTURN” formula?
--------
Regards,
Hide