This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWAVEICBOOST: It is suspected that the DC power socket on the board is abnormal. It is judged that there is a problem with the material

Part Number: MMWAVEICBOOST


Hi,

Input 5V, and the output of P3 terminal is only about 0.6V, but I didn't confirm how much voltage P3 terminal should output from the manual. Instead, I confirmed that the power output 5V is normal. After inserting into the power socket on the board, directly measure the DC power socket pin, and the measured voltage is 0.68v. It is suspected that the DC power socket on the board is abnormal. It is judged that there is a problem with the material.

Best regards,

Jiahui