Hi team,
My customer would like to know the max accuracy specification for this device down to the lower limit (-40°C). There is a graph with the typical, but no max accuracy spec.
Do we have this information handy?
Thanks,
Lauren
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
My customer would like to know the max accuracy specification for this device down to the lower limit (-40°C). There is a graph with the typical, but no max accuracy spec.
Do we have this information handy?
Thanks,
Lauren
Hi Josh,
In the EC table, it appears the max accuracy spec only goes down to 0 deg C. They're looking for -40 deg C.
Do we have the data for -40 deg C max accuracy spec?
Hi Lauren,
We cannot guarantee the RH accuracy of the device below 0°C.
If you look at the psychrometric chart for humidity, you can observe that the relative humidity converges to zero as the temperature goes below 0°C.
Regards,
Pavani Tenneti
Hi Pavani,
To clarify, my customer is asking the following-
"
I see this chart on the datasheet, p7:
And this specification from p5:
But, neither of these tell me the max temperature accuracy for the -40°C to +5°C range. We would need to know that for specification of that measurement in our own sensor, which does operate to the lower limit of -40°C.
"
Does that help? Let me know of your feedback.
Hello,
We cannot guarantee the temperature accuracy between -40°C and +5°C.
Regards,
Pavani Tenneti