Other Parts Discussed in Thread: IWR6843, MMWAVEICBOOST,
Hi,
Request advise on the following points
1. For IWR6843 what are the maximum and minimum value of S (slope of the f-t curve).
2. For IWR6843 what are the maximum and minimum value of Tc (Time observation window of the f-t curve).
3. Is it feasible to measure 1-10 micro-meter water surface vibration using IWR6843. I have IWR6843ISK-ODS and MMWAVEICBOOST available with me to try out. I worked out the calculations for Delta_pi as shown in the Video 1.2 of Intro to mmwave FMCW radar, it is coming to 0.144 deg for 1 micro-meter. Kindly advise on feasibility or things that needed to be done to achieve this.
Thanks.