Hello everyone,
i am having trouble getting the doppler_bins values using the rospkg in sdk 1.x and 2.x they were using dopplerIdx but seems like when i try to use it with sdk 3.x it gives back and error of range
my question here is can someone help me to get the values of doppler_bins on sdk 3.x what changes should be made in the ROS package because as i can see in sdk 3.x only x y z and Velocity are being returned and bearing range and doppler bins are always zero
Best regards