Other Parts Discussed in Thread: AWR2243
Following my previous question regarding the standard deviation of RF phase differences between two IWR1642 devices,
following a common SYNC_IN trigger:
1) Is the RF phase (and frequency) difference between the two presumably synchronized devices, small enough to enable
virtual channels, such that the transmission made by one IWR1642 device can be received and processed by the other IWR1642 device?
2) If so, can I cause one IWR1642 device to receive only, while the other IWR1642 transmits and receives?
3) If so, can I control which IWR1642 device transmits on which of its 2 antennas on a chirp by chirp basis?
4) If the answers to any or all the above are negative, can you recommend other TI devices which are more appropriate?
Thanks in advance.
Danny.