Other Parts Discussed in Thread: AWR2243, AM2732
Hello,TI's engineers:
I read the code about sdk4203 tdm mode.We use AWR2243 and AM2732 evm to develop radar.
Now i meet a question,see as follow:
#define DPU_RangeProcHWA_InputMode_MAPPED (uint32_t) 0U
#define DPU_RangeProcHWA_InputMode_ISOLATED (uint32_t) 1U
#define DPU_RangeProcHWA_InputMode_HWA_INTERNAL_MEM (uint32_t) 2U
There have three mode,but i can not understand what different about DPU_RangeProcHWA_InputMode_ISOLATED and DPU_RangeProcHWA_InputMode_HWA_INTERNAL_MEM .If we use AWR2243+AM2732,which mode should we selected.
Thank you very much!
BR
Bryant