This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: rlSetChannelConfig Error (RadarSS TX mailbox queue full)

Part Number: AWR2243


SPI Recv: 0xdcba abcd

              2032 004e 000c 0000 0003 df70

              1002 0024 0503 031a 6706 0000 0000 0000 019f 0000 fc30 0800 0000 0000 ffff ffff ffff 0000 1003 000c 0000 0000 0000 0000 1010 0010 0000 0000 0000 0000 0000 0000

              a740

Detail:rlCpuFault_t faultType=03 errorCode=05 lineNum=031a faultLR=00006706

Dear TI engineers, 

We met the difficult with error code 5, which means  (RadarSS TX mailbox queue full).  Please  check the upper error log. More details attached to the end of mail.

Could you tell me what conditions can caused the mailbox queue full?  and how to avoid the issue?

If you provide some advices, we will appreciated.

Thank you very much!

BRs

Zhang, Guoliang

=====Func:rlGetRfBootupStatus(0x01)=====
rlNonOsSemGet start
SPI Send: 0x1234 4321 0441 0014 3400 0000 0001 c7a9 0224 0004 9fc4 e048
rlNonOsSemGet start
SPI Send: 0x1234 4321 0441 0014 3403 0000 0001 c7a6 0224 0004 ffe1 6680
rlNonOsSemGet start
Debug Comment : MAX9295GpioCheck Pin Change PIN=0x0a Mode=0x01 (0x0->0x1)
RadSensCbInterruptHandler start
RadSensCbDeviceMaskHostIrq
SPI Send: 0x5678 8765 ffff ffff ffff ffff ffff ffff
RadSensCbDeviceWaitIrqStatus start(00)
Debug Comment : MAX9295GpioCheck Pin Change PIN=0x0a Mode=0x01 (0x1->0x0)
SPI Recv: 0xdcba abcd
0452 0024 3400 0000 0001 c788
0224 0014 fefb 073b 5079 0021 0010 0000 0000 0000
2fc7 c477
RadSensCbDeviceUnMaskHostIrq
rlNonOsSemGet start
RSS bootup status(0x01) : 0x073bfefb
=====Func:rlSetChannelConfig(0x01)=====
rlNonOsSemGet start
SPI Send: 0x1234 4321 0101 001c 4400 0000 0001 bae1 0080 000c 000f 0007 0002 0020 a439 7134
rlNonOsSemGet start
SPI Send: 0x1234 4321 0101 001c 4403 0000 0001 bade 0080 000c 000f 0007 0002 0020 19b1 23df
rlNonOsSemGet start
SPI Send: 0x1234 4321 0101 001c 4403 0000 0001 bade 0080 000c 000f 0007 0002 0020 19b1 23df
rlNonOsSemGet start
Debug Comment : MAX9295GpioCheck Pin Change PIN=0x0a Mode=0x01 (0x0->0x1)
RadSensCbInterruptHandler start
RadSensCbDeviceMaskHostIrq
SPI Send: 0x5678 8765 ffff ffff ffff ffff ffff ffff
RadSensCbDeviceWaitIrqStatus start(00)
Debug Comment : MAX9295GpioCheck Pin Change PIN=0x0a Mode=0x01 (0x1->0x0)
SPI Recv: 0xdcba abcd
2032 004e 000c 0000 0003 df70
1002 0024 0503 031a 6706 0000 0000 0000 019f 0000 fc30 0800 0000 0000 ffff ffff ffff 0000 1003 000c 0000 0000 0000 0000 1010 0010 0000 0000 0000 0000 0000 0000
a740
RadSensCbDeviceUnMaskHostIrq
RadSensCbAsyncEvent(Dev=0x01) usMsgId=0x0080 usAsyncSB=0x0002
[RadSensCbAsyncEvent](Dev=0x01)BSS CPU fault (RL_RF_AE_CPUFAULT_SB)
victor log:[CbAsyncEvent] Error is occurred (uiErrorCode=0x00000001, devIndex=0x01, usMsgId=0x0080, usAsyncSB=0x02, subLen=0x20,0503031a6706000000000000019f0000fc30080000000000ffffffffffff0000
victor log:Detail:rlCpuFault_t faultType=03 errorCode=05 lineNum=031a faultLR=00006706 faultPrevLR=00000000 faultSpsr=0000019f faultSp=0800fc30 faultAddr=00000000 faultErrStatus=ffff faultErrSrc=ff faultAxiErrType=ff faultAccType=ff faultRecovType=ff
RadSensCbAsyncEvent(Dev=0x01) usMsgId=0x0080 usAsyncSB=0x0003
[RadSensCbAsyncEvent](Dev=0x01)BSS ESM fault (RL_RF_AE_ESMFAULT_SB)
victor log:[CbAsyncEvent] Error is occurred (uiErrorCode=0x00000002, devIndex=0x01, usMsgId=0x0080, usAsyncSB=0x03, subLen=0x08,0000000000000000
victor log:Detail:rlBssEsmFault_t esmGrp1Err=00000000 esmGrp2Err=00000000
RadSensCbAsyncEvent(Dev=0x01) usMsgId=0x0080 usAsyncSB=0x0010
[RadSensCbAsyncEvent](Dev=0x01)Analog fault (RL_RF_AE_ANALOG_FAULT_SB)
victor log:[CbAsyncEvent] Error is occurred (uiErrorCode=0x00000004, devIndex=0x01, usMsgId=0x0080, usAsyncSB=0x10, subLen=0x0c,000000000000000000000000
victor log:Detail:rlAnalogFaultReportData_t faultType=00 faultSig=00000000
rlNonOsSemGet start
SPI Send: 0x1234 4321 0101 001c 4403 0000 0001 bade 0080 000c 000f 0007 0002 0020 19b1 23df
rlNonOsSemGet start