Hello,
A single-shot conversion happens when "Mode of conversion operation field" of the configuration register is configured as 01. But what if the register write happens before the completion of previous conversion? Such that a new write 01 command is sent 50ms after the firest one. Will the second command ignored or the first one will be ignored and the second one will be accepted?
Thank you.
Regards,
Oguri (TIJ automotive FAE)