Other Parts Discussed in Thread: TMAG5273
Hello
I am planning to use a DRV5056-A1 Hall sensor. The range of magnetic fields I will be detecting is North and South polarities in the 2-4mT range. Small magnets for a small product.
I considered using the DVR5055, bi-polar detector, these have 100mV per mT @5V sensitivity and are impossible to find these parts. Due to the low magnetic fields, I am decided to use the DRV5056, uni-polar, 200mV per mT @5V sensitivity
Questions
- See attached image. Can the DRV5056 be used to detect low magnetic fields? as shown by the "Operating Region"? Even North fields?
- See attached scope image (yellow trace) - this shows the actual output from the Hall sensor, where N and S magnetic fields are detectable. I just want to make sure its within the parts capability to detect a North field. If so where is it stated in the data sheet? I want to make sure I can get this response from the Hall sensor once we are in production.
- Considering I am detecting low magnetic fields, can you suggest another high sensitivity part? in a SOT23 package?
Thanks