Other Parts Discussed in Thread: TI-SCB, INA228, TMAG5170
Hi,
Currently I am evaluating the TMAG5170A1 device with TI-SCB using python script (UART, 921600) to readout and save data as mat file.
It seems that even though the device is configured as 4x - 3.1Ksps (3-axes) / 25mT / MAG_CH_EN = 9 (xyz), the readout speed is quite low (~500Hz for all 3 axis). Register 00-03 written to device are 0x2000, 0x25C0, 0x0200 and 0x0000.
May I know what is the maximum readout rate for this EVM?
Python script can be provided if needed.
Best,
Kit