This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: Read data from flash memory

Part Number: AWR1843BOOST
Other Parts Discussed in Thread: AWR1843

Hello everyone,

I am trying to use the primary bootloader of the AWR1843 radar, I connected an stm to the radar and sent some bytes using the write to flash command 

I checked with a logic analyzer and I got back an ACK response and a success response when I used the GET_Status command as well

then I tried to verify if those bytes I sent were received correctly in the flash memory of my AWR1843 so I used the QSPI driver and I I added the flash read function at the beginning of the MmwDemo_opensensor API in the MSS main like this :

I put a breakpoint there to be able to read the readBuf buffer which is the flash buffer but I keep getting an empty buffer 

PS : the EVM is in the functional mode of course when I am debugging 

any idea? thanks