I am using AWR1642BOOST ES1.0 for a demo. I need to configure the 1642 mss such that it applies default configuration as the demo, i.e. frame rate, resolution, range, velocity etc. in the mss without any host to configure at boot up and if possible use the sensor start/stop using GPIO to start and stop the point cloud data on the UART as there is limited numbers of UART available on the Host micro. Worst case I can live without the start stop if the sensor can configure itself and start transmitting the point cloud on the UART data port. Also does it need an ACK on each data packet sent? if so I will need to disable it in the mss too.
The demo sdk i.e. mmwave_sdk_01_02_00_05 does not include project files for me to open it using the CCS to modify the files and re-compile the project. I looked up the cloud and nothing exists for the the hardware version I have i.e. ES1.0.
If you have a binary already available to do the above, that will be great.
Kindly provide me the necessary ccs project that I can modify to achieve the above and the instructions for code modifications. Also confirm that the data structure of point cloud will be the same as what is in the docs folder of the sdk.
Much appreciated.
Regards,
Shyam